Flashed 13213-NCB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flashed 13213-NCB

2,421件の閲覧回数
xinr1b488
Contributor I
Hi, i just recently flashed my 13213-NCB network coordinator board, so i was wondering is there any chance to get back the message " Welcome to SND! PAN Coordinator." on the lcd? and of course the LEDs that are lighted when the SRB within the range. the same question goes out to 13213-SRB. Sensor reference board.
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,610件の閲覧回数
Mads
Contributor V
xinr1b488,
 
I think you need to elaborate a bit on what software your are running.
Our Beestack, MAC and SMAC demo applications does not display that message.
 
but if you are using an application generated from Beekit then you properly have to "enable" the display module.
 
BR,
Mads
0 件の賞賛
返信

1,610件の閲覧回数
xinr1b488
Contributor I
i've accidentaly flashed in the NCB, therefore it is not able to reusme it's previous functions, so is there any way to resume back the message of "Welcome to SND! PAN Coordinator." And yes, we are using the software BeeKit.
 
Thanks!
0 件の賞賛
返信

1,610件の閲覧回数
Mads
Contributor V
please tell me the name of the codebase you are using (and version) as non of our existing codebases prints out this message.
 
Br,
Mads
0 件の賞賛
返信