Flash Block Protection / Vector Redirection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flash Block Protection / Vector Redirection

3,697 次查看
gueggi
Contributor I

Hi,

i will used the 'FLASH Block Protection' and 'Vector Redirection' functionality of the MC9S08GB60A controller.

 

Questions:

- It is possible with this configuration to re-program the protected area?

- Is the 'Vector Redirection' available without 'Flash Block Protection'?

 

Thanks for your help.

 

Regards ...

标签 (1)
0 项奖励
回复
2 回复数

1,473 次查看
Alban
Senior Contributor II
Hi Again,
 
Q2- Is the 'Vector Redirection' available without 'Flash Block Protection'?
A2- in datasheet, answer is no.

Whenever any block protection is enabled, the reset and interrupt vectors will be protected. Vector redirection allows users to modify interrupt vector information without unprotecting bootloader and reset vector space. Vector redirection is enabled by programming the FNORED bit in the NVOPT register located at address $FFBF to zero. For redirection to occur, at least some portion but not all of the FLASH memory must be block protected by programming the NVPROT register located at address $FFBD. All of the interrupt vectors (memory locations $FFC0–$FFFD) are redirected, while the reset vector ($FFFE:FFFF) is not.
 
Alban.
0 项奖励
回复

1,473 次查看
Alban
Senior Contributor II
Hello !
 
Q1- It is possible with this configuration to re-program the protected area?
A1- Only after a mass-erase and un-secure of the Flash.
 
Cheers,
Alban.

Message Edited by Alban on 2006-11-06 04:17 PM

0 项奖励
回复