FXTH87 - Giving strange values sometimes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FXTH87 - Giving strange values sometimes

1,202件の閲覧回数
f20150335
Contributor III

Hi, I am using the FXTH87 TPMS for getting pressure readings through SPI on another device. I have disabled the RF module. But sometimes it gives very strange random values like Temperature as (-55), 110; voltage as 60 V etc and similar thing happens with the pressure readings as well.

What can be the causes behind these issues? Any suggestions are welcome. Thanks in advance.

ラベル(1)
0 件の賞賛
返信
0 返答(返信)