FSICE target CPU question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FSICE target CPU question

2,261 Views
trproc
Contributor I
I am trying to test a program using the FSICE with CodeWarrior 3.1. When starting the debugger, it asks for the target CPU and has a list of available CPUs. I am using a MC68HC908AS60A in a 52 pin PLCC package. On some of the other CPUs listed, there are versions shown for the PLCC and the QFP packages. The AS60A is only listed once with no package shown. Does anyone have any idea whether the FSICE is loading info for the PLCC or the QFP package?

Thanks
Labels (1)
0 Kudos
Reply
1 Reply

1,278 Views
Oliver
Contributor III
As far as I know the die is the same no matter what the package is. The Emulator Module uses the AS60 in the QFP package anyway to emulate your target CPU, there are just a few port pins not bonded out in the PLCC package, internally they are the same.

Best regards,

Oliver
0 Kudos
Reply