External inputs to a microprocessor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

External inputs to a microprocessor

跳至解决方案
1,727 次查看
barrygordon
Contributor I

I'm using a 9S08AC32 in my design.  The board that I'm designing has connectors that external modules can plug-in.  When the modules is inserted, it pulls an I/O pin of the micro (pull-ups enabled) low.  My logic detects if the I/O pin is low then a module is plugged in.  I have 16 of these input pins.  Normally I would route these pins to a parallel load serial shift register and clock the results in.  Hopefully the module would only be inserted in when the power is off.  The connector is pinned so the module can only be plugged in one way.  I have 16 spared I/O pins.

 

Any thoughts and/or opinions on this on going directly to the I/O's.

 

thanks,

 

    Barry

标签 (1)
0 项奖励
回复
1 解答
1,552 次查看
michaelsteffenf
NXP Employee
NXP Employee

Hi Barry,

There is no issues with connecting right to the microcontroller from the outside world, meaning the connector. The only thing that you will want to do is insert a 100 ohm resistor in series with all the spare i/o pins to limit any inrush current. Possibly add a 0.1uF cap to each line as well for filtering. We have many customers doing this in their designs as well.

Mike

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,553 次查看
michaelsteffenf
NXP Employee
NXP Employee

Hi Barry,

There is no issues with connecting right to the microcontroller from the outside world, meaning the connector. The only thing that you will want to do is insert a 100 ohm resistor in series with all the spare i/o pins to limit any inrush current. Possibly add a 0.1uF cap to each line as well for filtering. We have many customers doing this in their designs as well.

Mike

0 项奖励
回复