Example code for internal ADC of MC9S08DZ96

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example code for internal ADC of MC9S08DZ96

2,951件の閲覧回数
admin
Specialist II

I am evaluating MC9S08DZ96 for one of the application and interested in testing ADC performance before making decision on ADC and controller. I have evaluation kit with me, is there sample code for internal ADC of MC9S08DZ96, which can be used for basic evaluation testing purpose??

 

Thanks in Advance

Manoj

ラベル(1)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,815件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport


You can download the dz60_demo.zip from the following link:

http://www.axman.com/content/demo9s08dz60

Also you can check the samples that are install with CodeWarrior the normal folder is

C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.3\(CodeWarrior_Examples)\HCS08\Evaluation Board Examples\EVB9S08DZ60\C
These samples are for the Evaluation board but you can check the initialization and use it for the DEMO, I believe that the two board has the same package.
On this folder you can find a sample for CAN, LIN, SCI and the demo that use the ADC.

Best Regards,

Jennie

0 件の賞賛
返信

1,815件の閲覧回数
GMVS
Contributor III

hello

did you find anything useful?

i'm in the same situation...

regards

0 件の賞賛
返信