Error using SPI module in P89V51RD2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error using SPI module in P89V51RD2

1,235件の閲覧回数
avanishojha
Contributor I

Hi, I am trying to use P89V51RD2 controller for SPI module.

I have written

#include<intrins.h>

#include <P89V51Rx2.h>

sbit LE=P1^4;

sbit MOSI=P1^5;

sbit MISO=P1^6;

sbit clk=P1^7;

 

void main(void)

{

TMOD=0x20;//TIMER 1 MODE 2 AUTO RELOAD
TH1=0xFD;//9600 BAUD RATE @11.0592 mhZ

 

SCON=0x50;   // UART in Mode 1, 8Bit Data, 1Stop Bit, 1Start Bit

SPCTL= 0x51;

TR1= 1;
SPDAT=0x48;   // Place value in Buffer
while(SPCFG!=0x80);
SPCFG=0x00;

}

but I could not get anything on port pins MOSI or clk.

Please tell me What am I missing?

ラベル(1)
タグ(2)
0 件の賞賛
返信
0 返答(返信)