Error: Out of allocation space in segment ROM at address 0x7FD9

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error: Out of allocation space in segment ROM at address 0x7FD9

2,968 Views
Electrophile
Contributor I

Hi,

 

We are using recently released GW64 MCU and developed most of the code on CW6.2

 

After introducing irtc interrupt routines in the code, CW6.2 was giving us problems related to irtc write protect registers which we could not solve.

 

After discussing in detail with the FSL FAE's we decided to move to CW10.1 and ported whole code to CW10.1

 

Now we are stuck on this problem of "Out of allocation space in segment ROM at address 0x7FD9"

 

Being relatively new to FSL MCU's we are not sure of what to look at in the generated map file. Any comments/suggestions are welcome.

 

Thanks in advance for any help.

 

Cheers

DC

Labels (1)
0 Kudos
Reply
10 Replies

2,293 Views
CompilerGuru
NXP Employee
NXP Employee

Are you using the same prm as in 6.2?

Check the compilation options and the linker command line as well,

for example check that you are picking up the desired ansi library.

When creating the project with the 10.1 wizard, make sure to select the same options as with 6.2. For example enable floating point support can add a lot of code is you use a function out of the printf or scanf family (sprintf,...).

 

Daniel

0 Kudos
Reply

2,293 Views
Electrophile
Contributor I

Hi,

 

We have also tried building a new workspace using banked memory model.

 

It started giving fixup overflow in _Vector_52, to PDB_ISR type 1, at offset 0x0

 

After going through the forum threads discussing similar errors, we tried

 

#pragma push
#pragma CODE_SEG __NEAR_SEG PAGED_ROM
// interrupt handler here....
#pragma pop

 

for every ISR that was showing the problem.

 

We were able to sort our first few fixup errors.


Then we got stuck at a Fixup overflow error for a vector location which is not being used in our program

 

No luck :smileysad:

 

Hope, someone will help us understand and overcome this problem soon.

 

Cheers

DC

0 Kudos
Reply

2,293 Views
CompilerGuru
NXP Employee
NXP Employee

> Then we got stuck at a Fixup overflow error for a vector location which is not being used in our program

 

That's too little information to know what failed. Apparently something was using it, what was the failure message?

 

Anyhow, placing all interrupt handlers explicitely into non banked is a good idea for CW 6.2 or when using the small mm as well.

 

Daniel

 

0 Kudos
Reply

2,293 Views
Electrophile
Contributor I

> That's too little information to know what failed. Apparently something was using it, what was the failure message?

 

You are right Daniel, apparently one of our team members did wrote an ISR for that location and it was there all the time when we were trying to debug. I somehow missed it.

 

Thanks for pointing out.

 

No more fixup overflow problem now. Its the lauch configuration error :smileysad:

 

Cheers

DC

0 Kudos
Reply

2,293 Views
CrasyCat
Specialist III

Hello

 

Placing interrupt code in a section called PAGED_ROM is just confusing for everybody I think.

 

I would recommend you to fix the issue in 2 steps:

 

1- Place the interrupt functions code in a user define section called INTERRUPT_CODE for instance.

     This is done as follows:

    

#pragma push#pragma CODE_SEG __NEAR_SEG INTERRUPT_CODE// interrupt handler here....#pragma pop 

 

 

2- Place the INTERRUPT_CODE section appropriately in the .prm file.

    For this modify the placement block from

 

PLACEMENT /* Here all predefined and user segments are placed into the SEGMENTS defined above. */    DEFAULT_RAM,                        /* non-zero page variables */                                        INTO  RAM;    _PRESTART,                          /* startup code */    STARTUP,                            /* startup data structures */    ROM_VAR,                            /* constant variables */    STRINGS,                            /* string literals */    VIRTUAL_TABLE_SEGMENT,              /* C++ virtual table segment */    NON_BANKED,                         /* runtime routines which must not be banked */    DEFAULT_ROM,    COPY                                /* copy down information: how to initialize variables */                                        INTO  ROM; /* ,ROM1,ROM2: To use "ROM1,ROM2" as well, pass the option -OnB=b to the compiler */    PAGED_ROM                           /* routines which can be banked */                                        INTO  PPAGE_0,PPAGE_0_1,PPAGE_2,ROM1,ROM2;

 

    to

 

PLACEMENT /* Here all predefined and user segments are placed into the SEGMENTS defined above. */    DEFAULT_RAM,                        /* non-zero page variables */                                        INTO  RAM;    _PRESTART,                          /* startup code */    STARTUP,                            /* startup data structures */    ROM_VAR,                            /* constant variables */    STRINGS,                            /* string literals */    VIRTUAL_TABLE_SEGMENT,              /* C++ virtual table segment */    NON_BANKED,                         /* runtime routines which must not be banked */    INTERRUPT_CODE,    COPY                                /* copy down information: how to initialize variables */                                        INTO  ROM; /* ,ROM1,ROM2: To use "ROM1,ROM2" as well, pass the option -OnB=b to the compiler */    DEFAULT_ROM,    PAGED_ROM                           /* routines which can be banked */                                        INTO  PPAGE_0,PPAGE_0_1,PPAGE_2,ROM1,ROM2;

 

 

CrasyCat

0 Kudos
Reply

2,293 Views
Electrophile
Contributor I

Hello CrazyCat,

 

I tried your suggestion, with this suggestion fixup overflow error is coming in normal function calls.

E.g..: Fixup overflow in Set_TimeOut_MTIM1, to Disable_MTIM1 type 3, at offset 0x5

 

Both Set_TimeOut_MTIM1 and Disable_MTIM1 are simple timer init function calls

 

Do you think we might have allocated too much contiguous memory space to INTERRUPT_CODE.  0x1960 TO 0x7FFF is about 26KBytes out of 64KBytes!

 

Would you suggest judicious use of paged memory section ,by allocating them like this

 

INTERRUPT_CODE_SECTION_1, COPY  PPAGE_0

INTERRUPT_CODE_SECTION_2, COPY  PPAGE_0_1

INTERRUPT_CODE_SECTION_3, COPY  PPAGE_2

 

instead of

 

INTERRUPT_CODE,    COPY        INTO  ROM;

 

in the prm file?

 

Consequently pragma directives will need to be updated accordingly.

 

Cheers

DC

0 Kudos
Reply

2,293 Views
CompilerGuru
NXP Employee
NXP Employee

Interrupt handles themselves must be non banked as the vector table just takes 16 bit vectors.

However any other functions can be allocated banked, and if you happen to have some huge interrupt handlers you can move those into normal functions and call them from a trivial interrupt handler (will slow it a bit down, of course).

Do your interrupt handlers themselves use 26k?

 

Also note that this fixup overflow is a different type than the prior ones. Has been a while, but could it be that you allocate the section containing both Set_TimeOut_MTIM1 and Disable_MTIM1 into 2 separate segments?

Say, something like

 

MY_SECTION        INTO  ROM, ROM1;

 

For that to work, please add the -OnB=b compiler option (many prm files contain a note stating that too).

 

The COPY section must be the last one placed in a non banked segment.

 

Daniel

0 Kudos
Reply

2,293 Views
CrasyCat
Specialist III

Hello

 

I assume you are building code in banked memory model.

Is that correct?

 

Can you check preprocessor listing in file where Set_TimeOut_MTIM1 is implemented.

 

Do you have a prototype for Disable_MTIM1 in there? What is the latest pragma CODE_SEG preceding the prototype?

 

CrasyCat

0 Kudos
Reply

2,293 Views
CrasyCat
Specialist III

Hello

 

Where is PAGED_ROM allocated in the .prm file?

Should be placed in NON_BANKED memory.

 

CrasyCat

0 Kudos
Reply

2,293 Views
Electrophile
Contributor I

@ Daniel: We are using CW 10.1 at the moment because of some irtc related issues in CW6.2 especially with GW64 MCU. We are not even able to use any basic irtc drivers in CW 6.2 IDE. Thats why we ported our whole code to CW 10.1

 

Hi Crazycat,

 

I feel that is where the problem is. Issue is with our understanding of the prn file.

 

Attached is the original unmodified prn file. I am confused about where and what to modify to place PAGED_ROM in NON_BANKED memory area.

 

We did a few experiments with the prm file. Now we are not getting any errors. But, we are stuck at launch configuration error just after initiating debug mode.

 

also tried disabling -OnB-b optimization. No luck :smileysad:

 

I really appreciate the help you guys extend to the freescale forums. God bless you all.

 

cheers

DC

0 Kudos
Reply