Enable Events on CodeWarrior v5.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enable Events on CodeWarrior v5.0

4,124件の閲覧回数
Zampo
Contributor I
Hi, I can't enable Events when I'm setting the bean "capture";
 I can't modify anithing in bean inspector->Events...Please help me
my project is stuck
 
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,203件の閲覧回数
Zampo
Contributor I

:smileyhappy:

Last message was useful to solve my problem....

I have never noticed this button.....

I'm a newbie

 

Now I can Work

 

Bye bye Thanx

0 件の賞賛
返信

2,203件の閲覧回数
Zampo
Contributor I

Thank for your reply!

I'm targetting MC9S08GB60CFU.

I'have followed your hints but in Bean Inspector:InputCapture Properties event enabled is set "YES" but in grey color and I can't modify it. In the window Events I can't' set any events. Everyone is set as "don't' generate code".

Thanks

Zampo

0 件の賞賛
返信

2,203件の閲覧回数
ProcessorExpert
Senior Contributor III
To enable events at Events page it is necessary to set "Interrupt service/event" property at Properties page to value "yes". You probably modified the "Event enabled" property used for enabling events during peripheral initialization.
 
I hope this help you.
 
Best Regards, Jan Pospisilik, Processor Expert Support
0 件の賞賛
返信

2,203件の閲覧回数
CrasyCat
Specialist III

Hello

Which MCU are you targeting (HCS08GB60, ....)?

I assume you are trying to use the Capture Bean. Am I right?

I would set "Interrupt service/event" to Enable in the Capture Bean property and then You should be able to enable separate event in the Event Tab.

CrasyCat

0 件の賞賛
返信