Embedded DEMOQE BDM is a full Multilink?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Embedded DEMOQE BDM is a full Multilink?

22,236 Views
carloscuev
Contributor V
I have the DEMOQE Board, it says it has a embedded USB Multilink. In fact it installs with USB Multilink Drivers.
I have tried to program a QG8 (through an aux bdm 3x2 header)  and it didnt work :smileysad:

The question is... Is it possible? Or embedded USB Multilinks are limited to a single chip/family ?

Thank You very much
Labels (1)
0 Kudos
Reply
32 Replies

10,270 Views
carloscuevas
Contributor III

Sorry, that URL I have is on my web server and I changed domain name and didnt make the appropiate forwards. here is the link again:

 

http://escalalibre.com/descargas/P&E_DLLs.zip

 

Hope you find it useful

0 Kudos
Reply

10,270 Views
pierpd
Contributor I

Hi folks,

 

this is just to notify that those DLLs solved my problem with the HCS08QE32 in the LQFP package (32 pins).

 

I am using the USB Multilink to program the chip and CW 6.2, but without those DLLs it was not working (I could not program the micro at all). The strange fact is that I could program the same chip in the QFN-48pins package...

 

Anyway, thank you for the help!

 

Pierpaolo

0 Kudos
Reply

10,270 Views
naej_gz
Contributor I

Hy

 

Changing limitations of an existing product is very unfair from P&E

I  bought 12 demo board QG8 for the school last year.

Had I knew this before ...

 

bye jean

0 Kudos
Reply

10,270 Views
dongustavo
Contributor I

Hello all,

 

I´m trying to do so from 6.1 to 6.3 

DEMOQE to program 9s08SE4 device...

 

Any comments?

 

 

0 Kudos
Reply

10,270 Views
dongustavo
Contributor I

I get this:

 

Loading Target ...
Windows NT detected.
USB HCS08/HCS12 MULTILINK detected - Flash Version 5.81
Frequency change to ~4505212hz.
USB HCS08/HCS12 MULTILINK detected - Flash Version 5.81
Error: Can not enter background mode.
USB HCS08/HCS12 MULTILINK detected - Flash Version 5.81
Device is 9S08SE4.
Mode is In-Circuit Debug.
IO registers loaded for MC9S08SE4 from C:\Archivos de programa\Freescale\CodeWarrior for Microcontrollers V6.3\prog\REG\MCU1061.REG
No Link To Target

 

Loading Target ...Windows NT detected.USB HCS08/HCS12 MULTILINK detected - Flash Version 5.81

Frequency change to ~4505212hz.

USB HCS08/HCS12 MULTILINK detected - Flash Version 5.81
Error: Can not enter background mode.


USB HCS08/HCS12 MULTILINK detected - Flash Version 5.81Device is 9S08SE4.Mode is In-Circuit Debug.IO registers loaded for MC9S08SE4 from C:\Archivos de programa\Freescale\CodeWarrior for Microcontrollers V6.3\prog\REG\MCU1061.REG

No Link To Target

 

I´m stuck on this.

0 Kudos
Reply

10,270 Views
peg
Senior Contributor IV

Hello

 

I was just looking for this thread to explain your previous post when the notification for your above post arrived.

I am quite sure the problem you have is as described here.

The fix described here should work also.

 

0 Kudos
Reply

10,270 Views
BobbyMK
Contributor I

Hi 

I have been reading the thread and wanted to know if anyone know if it is possible to use the BDM connector on the DEMOQE board to program an external MCF51QE128. I tried installing codewarrior 6.2 and over writing the DLLs as you suggested but I still get the following error:

 

"The target MCU is not responding. Please turn MCU power off and on, and click ok. This will atempt to enter debug mode througha power on reset sequence (BKGD is currently driven low)"

 

Any help or insight would be much appreciated.

Bobby

0 Kudos
Reply

10,270 Views
carloscuev
Contributor V

Try replacing the whole bunch of DLLs from here

I have uploaded that ones just for you :smileywink:

Try them on CW 6.3.1 only, v6.3 wont do.

They are 6.3.1 DLLs, not renamed 6.1 DLLS as last time.

You can program any other micro (RS08 only if you provide the VPP) with your DEMOQE

Note: only DEMOQE, not DEMOJM, neither other one.

 

0 Kudos
Reply

10,270 Views
MICROAR
Contributor I

JUST DO NOT BUY ANY P&E PRODUCT:

 

LIMITATIONS OF THEY PRODUCTS ARE NOT CLEAR.

 

BUY OR MAKE YOUR SELF A OPENBMD.

 

0 Kudos
Reply

10,270 Views
carloscuev
Contributor V

In fact, I got 3 USBDMs from eBay, 25 bucks each one, USB Flash drive size, they ROCK big time 

Very happy with them :smileyvery-happy:

0 Kudos
Reply

10,270 Views
snicolas
Contributor I

Hi @carloscuev,

 

does your new OSBDM work fine on CodeWarrior 10.x?

 

Could you share the eBay link?

 

Thanks 

0 Kudos
Reply

10,270 Views
rak63
Contributor I
Hi Carlos!

Y try it with a AW60 and it works fine with the QG8 demo & CW6.2 with 6.1 dlls.

Thank you!

Regards

Roberto

Bs. As. - Argentina

Message Edited by rak63 on 2009-02-26 11:17 AM
0 Kudos
Reply

10,270 Views
carloscuev
Contributor V
Well, HCS12 devices will need another hack in CW HCS12 Edition. I hope this hack can be ported very similar for HCS12 version

0 Kudos
Reply

10,272 Views
carloscuev
Contributor V
I would like some of you testing this hack to program HCS12 and RS08 uC's
I'm having some RS08 next week. I'll try directly with embedded multilink alone and also with external 12v source (maybe a maxim capacitor pump, i like those :smileywink: )
0 Kudos
Reply

10,272 Views
carloscuev
Contributor V
CW3.1 has 1.26, 1.29, 1.35
CW5.0 has 1.37
CW5.1 has 1.40
CW6.0 has 1.49
CW6.1 has 1.54
CW6.2 has 1.56

In order to replace succesfully the CW6.1 (v1.54) files in CW6.2 they have to be renamed with the original name in CW6.2, that is:

ICD08z_dll_v156.dll
ICDrs08_dll_v112.dll
prog08z_dll_v156.dll
progrs08_dll_v112.dll

:smileyvery-happy: it REALLY works. In fact I'm programming right now QG8 in CW6.2 using embedded Multilink in DEMOQE :smileyhappy:

With original DLLs I couldnt. With CW6.1 DLLs now i can. :smileyvery-happy:

Its running flawlessly !!!


Message Edited by carloscuev on 2009-01-07 11:46 PM
0 Kudos
Reply

10,272 Views
sebasira
Senior Contributor I

Hello! I'm having the same problem with demoJM.. I wan't to programm a QE MCU...

 

I have win7 x64... To make older version of codewarriro work over win7 you must copy CodeWarrior from an installed version on win XP. Then set a file to be compatible win XP SP2 and run register it. I've done this with CW6.1 CW6.2 and CW6.3...

Then, as this thread says, I copy and rename the four files to have the same name as the one in each installation. But I still can not load code to QE...

 

OVER WIN 7 x64

*******************

- With CW6.1 ----> Embedded Multilink cannot be detected by the Connection Manager

- but with both CW6.2 and CW6.3 ---> The Connection Manager detects the Embedded Multilink but cannot load code to the target

 

 

So then I tested over win XP

 

 

OVER WIN XP x32

********************

- With CW6.1 ----> Work just fine

- but with both CW6.2 and CW6.3 ---> The Connection Manager detects the Embedded Multilink but cannot load code to the target

 

 

Something is not rigth here... Why would the DEMO JM board function as a BDM over win XP and not over win 7? Both PC has the latest version of P&E driver...I'd like to add that CW6.1, 6.2 and 6.3 running over win7 are the copy of the installed one on win XP.

 

One more thing I've just notice. CW6.1 has Connection Manager v1.04.00.01, and the other 2 have the v3.30.00.00 and v3.55.00.00

 

The problem is that CW6.1 over win 7 cannot detect the DEMO JM Embedded Multilink... It would be enough to make CW6.1 detect this board over win7 to solve my problem

 

Please any help would be greatly appreciatted!!

Thank you all!!

 

0 Kudos
Reply

10,272 Views
peg
Senior Contributor IV
OK, that clears it up.
Good work!

Now all that is needed is a reason why this is so from Freescale/P&E.



Message Edited by peg on 2009-01-08 11:33 AM
0 Kudos
Reply

10,272 Views
carloscuev
Contributor V
After some research and empiric tests I've managed to find a solution:

Simply put this DLLs:
http://freescale.teknoplex.com/descargas/P&E_DLLs.zip

Inside Here:
C:\Program Files\Freescale\CodeWarrior for Microcontrollers V6.2\prog\P&E\

Be sure to backup original Files !

Enjoy!


Message Edited by carloscuev on 2009-01-21 01:49 AM

Message Edited by carloscuev on 2009-01-21 01:49 AM
0 Kudos
Reply

10,272 Views
peg
Senior Contributor IV
Hello Carlos,

Just for reference I searched my computer for prog08*.dll
I have installed:
CW3.1, CW5.0, CW5.1, CW6.0 and the standalone version of the Expert mode programmer that is included within CW.
This DLL appears only to be associated with Codewarrior and not the standalone application.
These are the version numbers:
CW3.1 has 1.26, 1.29, 1.35
CW5.0 has 1.37
CW5.1 has 1.40
CW6.0 has 1.49

The zip file you attached is named 1.54 but inside is 1.56. Where is your mistake?
Perhaps you could fill in the rest of my table above.

0 Kudos
Reply

10,272 Views
peg
Senior Contributor IV

Hello all,

 

The previously attached file seem to have disappeared. (I think there over behind that grassy knoll)

I have attached them here separately this time as Freescale have reduced the max file size.

 

ICD08z_dll_v156.zip

prog08z_dll_v156.zip

Message Edited by t.dowe on 2009-09-08 09:33 AM
0 Kudos
Reply