EEProm S08PT16

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EEProm S08PT16

1,005件の閲覧回数
IlConte
Contributor IV

I have a question about the code position for read/write eeprom.

In such cases I have to run the code from RAM ?

I have read the datasheet (Table4-18) and AN4570, but remain a doubt :

When the code is mormally execute in flash, can i read the eeprom value ?

The Program flash Read is considerated also when the code in flash is executed ?

 

17153_17153.pngpastedImage_0.png

 

Thanks

 

Stefano

ラベル(1)
0 件の賞賛
返信
0 返答(返信)