EEProm S08PT16

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EEProm S08PT16

1,006 次查看
IlConte
Contributor IV

I have a question about the code position for read/write eeprom.

In such cases I have to run the code from RAM ?

I have read the datasheet (Table4-18) and AN4570, but remain a doubt :

When the code is mormally execute in flash, can i read the eeprom value ?

The Program flash Read is considerated also when the code in flash is executed ?

 

17153_17153.pngpastedImage_0.png

 

Thanks

 

Stefano

标签 (1)
0 项奖励
回复
0 回复数