Downloading with Serial Monitor M68DEMO908GB60, but use SCI1 for me applicaction

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Downloading with Serial Monitor M68DEMO908GB60, but use SCI1 for me applicaction

1,728件の閲覧回数
mvergaracid
Contributor I
Hi:
 
I'm new with the Freescale.
I can upload my application using the Serial monitor. I need use both SCI1 & SCI2. All is right with the SCI2, but the SCI1 is not receiving and sending data.
I only want downloading my application to the HCS08, not enter in debug mode.
Somebody can give me a light ?
 
Best Regards,
 
Mauricio.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,010件の閲覧回数
ang
Contributor I
Hi
 
you are using seral monitor for downloading your application right?? So please check which is the serial channel used by the serial monitor. if serial monitor is using the SCI1 interrupt, you can't use SCI1 interrupt  in your application.
regards
ang
0 件の賞賛
返信

1,010件の閲覧回数
mvergaracid
Contributor I
I forget:  I'm using Processor Expert to the development of my Application.
Best Regards,
 
Mauricio.
0 件の賞賛
返信