Download apps without BDM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Download apps without BDM

ソリューションへジャンプ
2,661件の閲覧回数
Loris83
Contributor II

I'm using MC1321x EVK.

I don't have a BDM.

Is possible uploading apps without using BDM?

I've read many discussions like this:

 

http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&thread.id=3336

 

but nothing certain.

 

Someone could help me?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,981件の閲覧回数
peg
Senior Contributor IV

Hello and welcome to the fora, Loris.

 

Yes you can use a bootloader but you need to be able to programme the bootloader code in to your device first. For this you will need a BDM. The bootloader is some code that will remain within the device and talk to your computer over a serial port. It recieves and programmes your code and erases your code when required but does not erase itself.

The main problem is the Catch-22 in the first place.

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,982件の閲覧回数
peg
Senior Contributor IV

Hello and welcome to the fora, Loris.

 

Yes you can use a bootloader but you need to be able to programme the bootloader code in to your device first. For this you will need a BDM. The bootloader is some code that will remain within the device and talk to your computer over a serial port. It recieves and programmes your code and erases your code when required but does not erase itself.

The main problem is the Catch-22 in the first place.

 

0 件の賞賛
返信
1,981件の閲覧回数
Loris83
Contributor II

So I need a BDM to work with this kit.

 

Thanks

 

Loris

0 件の賞賛
返信