Download apps without BDM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Download apps without BDM

跳至解决方案
2,665 次查看
Loris83
Contributor II

I'm using MC1321x EVK.

I don't have a BDM.

Is possible uploading apps without using BDM?

I've read many discussions like this:

 

http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&thread.id=3336

 

but nothing certain.

 

Someone could help me?

标签 (1)
0 项奖励
回复
1 解答
1,985 次查看
peg
Senior Contributor IV

Hello and welcome to the fora, Loris.

 

Yes you can use a bootloader but you need to be able to programme the bootloader code in to your device first. For this you will need a BDM. The bootloader is some code that will remain within the device and talk to your computer over a serial port. It recieves and programmes your code and erases your code when required but does not erase itself.

The main problem is the Catch-22 in the first place.

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,986 次查看
peg
Senior Contributor IV

Hello and welcome to the fora, Loris.

 

Yes you can use a bootloader but you need to be able to programme the bootloader code in to your device first. For this you will need a BDM. The bootloader is some code that will remain within the device and talk to your computer over a serial port. It recieves and programmes your code and erases your code when required but does not erase itself.

The main problem is the Catch-22 in the first place.

 

0 项奖励
回复
1,985 次查看
Loris83
Contributor II

So I need a BDM to work with this kit.

 

Thanks

 

Loris

0 项奖励
回复