Digianswer A/S Freescale 802.15.4 Analyzer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Digianswer A/S Freescale 802.15.4 Analyzer

1,777 Views
ve3id
Contributor III

Hi all,

I have a Freescale 802.15.4 analyser that came  with the Zigbee developer's kit back in 2004/5 or so.  I am working on an 802.15.4 project with some FRDM-K64s and need a sniffer.  The software that came with it was installed on a long-lost XP machine and now I am trying to use it with that software, made by Frontline Test Systems.

Problem is it needs an online key to run it.  Frontline no longer support it. I don't care for the software since I only use linux, but does anybody know of any software that uses it. or Is there a driver for linux so that I can use it with Wireshark?  It responds to lsusb as ID 08fd:f001 Digianswer A/S Freescale 802.15.4 Analyzer

Any help greatly appreciated!

 

cheers,

Nigel

 

 

0 Kudos
Reply
1 Reply

1,705 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,  

 

As the device that you are mentioning are quite old, I believe that the following would be all we have available BeeKit Wireless Connectivity Toolkit | NXP Semiconductors .

Please consider that this SW is no longer supported 

 

Regards

0 Kudos
Reply