Demo QE board and BDM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Demo QE board and BDM

2,503 Views
maverick
Contributor I
Hello,

My question is: can I use the Demo QE board's BDM to program any other S08 or S12X? Or is it limited to flexis microcontrolers.

Thank you in advance.

Mav
Labels (1)
0 Kudos
Reply
1 Reply

1,030 Views
JimDon
Senior Contributor III
Add the 6 pin header, get a 6 pin IDC cable, and you are ready to rock.

It is a a full P&E BDM and will work with CFV1, S08 and S(X)12 boards.

However, do not expect it to supply power to the board. I have been told it is also not as well protected and a USB 12 is - not sure what that means.
0 Kudos
Reply