Dear Expret.     I need you help about MC9S08AC60 problem...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dear Expret.     I need you help about MC9S08AC60 problem...

1,590件の閲覧回数
waan
Contributor I
Dear Expret.
    I need you help about MC9S08AC60 problem.Now I use this mcu to design washing machine and it has problem about data in flash program area is loss when I run machine around 2 day continue.
At this problem I use 6 machine for test and 2 machine has this problem.In design I use virtual EEPROME at address 0870 to 0A70 and Program memory at address 1860 to FFFF.in this problem data is loss at  Program memory area and it random address.
Pls help me to find a root of this problem.
Thank you .
Narongsak Metta.
ラベル(1)
0 件の賞賛
返信
1 返信

965件の閲覧回数
Quasar
Contributor I
Hi Waan,
 
Are you trying to write data into flash ?
I don't know if this will help you ... but from my experience (an unpleasant one), once, I think two year ago, I've done a mistake into a program which save a variable into a eeprom at a specific time interval. I've forgot about it, and when i made the burn-in tests of the device i was surprised to see the processors were damaged after a while (something like in your case).
I may case the root cause was simple ... writing in Flash or eeprom is allowed only for a limited time.
 
 
 
0 件の賞賛
返信