DEVELOP BOARDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DEVELOP BOARDS

3,151件の閲覧回数
rdavila
Contributor I
HI ! I WOULD LIKE TO KNOW WHICH IS THE BEST DEVELOPMET BOARD FOR HC08 GP32... WHEN I MEANT THE BEST I MEAN PRICE, EASY TO USE. THANKS I HOPE SOMEONE CAN HELP ME.

(I KNOW THAT FREESCALE HAS SEVERAL BOARDS BUT I CANT EVALUATE THEM, IF YOU'RE ABLE TO HELP ME I'LL BE GRATEFUL)
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,604件の閲覧回数
peg
Senior Contributor IV
Hi rdavila,
 
If you think the GP32 is what you want then I would suggest looking at the 9S08GT32.
It has pretty much the same I/O but is S08 so has BDM access and much faster.
 
I have converted a couple of applications from GP32 to GT16 and will never look back!
 
This way you could go with a GB60 DEMO board. A GTxx is a cut down (less pins) version of a GBxx
 
Regards
Peg
0 件の賞賛
返信

1,604件の閲覧回数
OldMan
Contributor I
I think GB60A is better than GB60. So are GB32A, GB16A, GB8A, GT60A, GT32A, GT16A, and GT8A as compared with the corresponding non-A parts.
 
Also MEMO board for GB60 is no longer in production.
 
Please check it out and do not rely on my words.
0 件の賞賛
返信