DEMOQE BDM Functionality questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DEMOQE BDM Functionality questions

2,898件の閲覧回数
protoease
Contributor II
I bought one of the DEMOQE boards made by P&E and distributed by mouser et. al for $50. 

My question is, if I install the 6-pin header and use this board to program external target boards, will it support voltage level translation for, lets say a AW32 processor running at 5V.  The QE board runs at roughly 3 Volts, but it does have a battery to power the board from, so I would assume this would mean that the USB-BDM that is on the backside of the board would have to have some kind of level translation to allow the variable voltage.  I'm just not sure how high this can go.

Would appreciate any advice.

Thanks,
Aaron
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,921件の閲覧回数
BobbyMK
Contributor I

Hi

Just wanted to know if you were able to get the DEMOQE to program an external MCF51QE128 via the BDM connector.

Thanks for any help.

Ada,

0 件の賞賛
返信

1,921件の閲覧回数
protoease
Contributor II
Finally tried it out, I just installed 5 pins the 6 pin BDM header onto the DEMOQE board (I didn't install a pin in the VDD line) and it programmed and debugged my protoboard built QG8 prototype just fine.

This is a good way to get what seems to be the full functionality of the PE BDM pod at about half the cost.  The only thing in my mind that you are lacking is a nice case.
0 件の賞賛
返信

1,921件の閲覧回数
JimDon
Senior Contributor III

It also can not program the KA series, because it needs 12v vpp. Supposedly it is also not as well protected as the USB Mulitlink.


0 件の賞賛
返信

1,921件の閲覧回数
JimDon
Senior Contributor III

I have it used to to debug +5 V hcs12 boards. So I would say yes. Needless to say to NOT connect the VSS pin.


0 件の賞賛
返信