DEMOJM Board USB Resume Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DEMOJM Board USB Resume Issue

1,069件の閲覧回数
huachun
Contributor I

I am using MC9S08JM60 with DEMOJM board. It seems there is a problem with HID mouse example code in the disk.

 

HID mouse code works well when I connect the board to PC. But if I set PC to standby mode and then back to normal mode, device is not resumed successfully. Digged into the code, I found that MCU went back to STOP3 mode after failed waiting for RESUMEF which is supposed to be valid at that time. After that MCU will never come back to normal mode. Onlyl if I change the code to not go to STOP3 mode again if the RESUMEF is not valid, then it works.

 

I have also measured the external clock signal. When the USB resume signal triggered MCU from STOP3 to normal mode, there is no output from external clock. I guess MCU went to STOP3 mode again before successfully switch clock.

 

What caused USB resume fail? Is it because of the clock issue? How to solve this properly?

Thanks.

Regards,

Huachun

ラベル(1)
0 件の賞賛
返信
0 返答(返信)