DEMO9S08LC60 stuck!! help!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEMO9S08LC60 stuck!! help!

1,337 Views
p5yc0d3
Contributor I

My DEMO9S08LC60 got stuck when I loaded a programm, how can I return the state of my DEMO9S08LC60  to default? I have pressed the reset button but it doesn't work!. and i can't load new programs because appears a window saying that there are not connection. I hope someone can help me!

Labels (1)
0 Kudos
Reply
1 Reply

1,238 Views
LucasB
Contributor I

 

Hello ... I would love to help but I have the same problem and for days I'm trying to solve.
When I connect the debug board to try to connect but then jumps me an error saying that at this moment is this ejecuntando if I want to stop, when I put it if I said that it was not possible. As I watched I suspect can not estop the board or there is a problem with thereset. You might have accidentally stepped on the IVT?

 

0 Kudos
Reply