DEMO9S08JS16 - hybrid USB peripheral?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEMO9S08JS16 - hybrid USB peripheral?

Jump to solution
7,277 Views
irob
Contributor V

Hello, I'm using the DEMO9S08JS16 and going through the labs now.  Pretty nice little micro.

 

There is included a lab and source code for turning the micro into a USB mouse and another for USB keyboard, using the HID standard.

 

My question is, could it be possible to use both at the same time with HID, such that some buttons would be mouse control and others keyboard keys?  Anyone tried this?

Labels (1)
0 Kudos
Reply
1 Solution
4,155 Views
Tsuneo
Contributor IV

Increase the wMaxPacketSize for the interrupt IN endpoint into 9.

It is assigned HID_INT_IN_EP_SIZE macro

 

 

Hid.h#define HID_INT_IN_EP_SIZE      9

Where did you change?

On the trace, the device still returns the input report without any report ID.

Revise your code so that you see this report format on the trace.

 

 

For keyboard,offset (byte) 0       report ID (01) 1       modifier keys 2       padding 3 - 8   keycode arrayFor mouse,offset (byte) 0       report ID (02) 1       buttons 2       X asis 3       Y axis

 

 

You run USBlyzer and SnifUsb (usbsnoop) at the same time.

It causes the trace complicated.

 

Tsuneo

 

View solution in original post

0 Kudos
Reply
16 Replies
4,155 Views
irob
Contributor V

My goal here is to make a composite HID device, a mouse & keyboard, using the MC9S08JS16.  My platform for testing is the DEMO9S08JM board with JS16 module plugged in.

I started with the demo kit's example HID keyboard and mouse projects.  Nice software, but by no means non-trivial!  From what I've read elsewhere, the best approach would be to make a single endpoint with two interfaces.  I've begun this, but would appreciate anyone's input.  I've attached the project so far, which is far from compiling.



(UPDATE)

 

I now have both mouse and keyboard HID descriptors concatenated into one HID_RPT, by using 2 report IDs.  See here for more info.  However, data buffers are no longer sent to the host PC, and I'm not sure why.

 

Attached is the updated software.

0 Kudos
Reply
4,155 Views
irob
Contributor V

I have recently discovered that the added ReportID lines in the descriptors (Usb_Descriptors.c) are what causes the data buffers to disappear.

 

As a simple test, I took the keyboard-only HID sample code, added the ReportID line.  The host will continue to register this device correctly as a HID keyboard.  But none of the data buffers will make it to the host (pressing keys results in nothing to the PC).

 

So the data buffer routines must need some more work to handle the added ReportIDs

0 Kudos
Reply
4,155 Views
admin
Specialist II

Are you the same one who posted to SiLabs USB forum about multiple TLCs (Top-Level Collections) of keyboard and mouse?

http://www.cygnal.org/ubb/Forum9/HTML/001496.html

 

 


irob wrote: 

As a simple test, I took the keyboard-only HID sample code, added the ReportID line.  The host will continue to register this device correctly as a HID keyboard. 


After changing the report descriptor, delete (uninstall) the device once on the device manager, or USBDeview, unless the VID/PID of the device is also changed. And then, the device is recognized as both of keyboard and mouse.

http://www.nirsoft.net/utils/usb_devices_view.html

 

 


irob wrote:

 

So the data buffer routines must need some more work to handle the added ReportIDs


 

 

You are right.

As I wrote on above SiLabs post, each input report has to be preceded by the report ID.

 

Tsuneo

0 Kudos
Reply
4,155 Views
irob
Contributor V

Tsuneo, I have prepended the report ID (0x01 or 0x02 for my keyboard or mouse) into the function HID_Transfer_Rpt()  which is in hid.c.

 

Unfortunately, the host PC is still not seeing data.  I also tried prepending the ReportID keyword code of 0x85, thinking maybe that was required.

 

HC08 is big endian and the PC is little endian.  I thought maybe I should reverse the position of the Report ID in my data buffer.  Tried that, still didn't work.  Hmm.

0 Kudos
Reply
4,155 Views
Tsuneo
Contributor IV

 

Monitor USB traffic using a hardware USB analyzer or software sniffer.

Is the host reads out the input report from the interrupt IN endpoint?

 

For software sniffers,

If BulkOrInterrupt request is held in pending, the firmware doesn't put the report to the endpoint correctly.

If the request fails, the endpoint is not initialized well.

If the request success, but the host app doesn't see the report, the report format (usually report length, or report ID) is wrong.


Software sniffers

SniffUsb (open source) http://www.pcausa.com/Utilities/UsbSnoop/default.htm

USBlyzer (with free trial) http://www.usblyzer.com/

HHD USB monitor (with free trial) http://www.hhdsoftware.com/Downloads/usb-monitor.html


Tsuneo

0 Kudos
Reply
4,155 Views
irob
Contributor V

Tsuneo, you've been a big help.  I took your advice and am running USBlyzer now.  It is showing me some interesting things.  For one, I see that the the Input Report length is still only 8 bytes, though I've increased the buffer size in software to 9 bytes (to include the ReportID).  USBlyzer shows a buffer length of 9, but an Input Report of only 8.  See below...

 

Capture List

START000114:39:14.049









URB000214:39:16.034Bulk or Interrupt Transfer9 bytes buffer
in01:00:81892EB878h
usbsnoop89381BB0h
URB000314:39:16.034Bulk or Interrupt Transfer9 bytes buffer
in01:00:81892436C0hUSBPDO-8
89381BB0h
URB000414:39:16.143Bulk or Interrupt Transfer9 bytes buffer
in01:00:81892EB878h
usbsnoop89480B80h
URB000514:39:16.143Bulk or Interrupt Transfer9 bytes buffer
in01:00:81892436C0hUSBPDO-8
89480B80h
URB0006-000314:39:18.768Bulk or Interrupt TransferInput Report len:800 00 4F 00 00 00 00 00in01:00:81892436C0hUSBPDO-8
89381BB0hSuccess (Success)
URB0007-000214:39:18.768Bulk or Interrupt TransferInput Report len:800 00 4F 00 00 00 00 00in01:00:81892EB878h
usbsnoop89381BB0hSuccess (Success)
URB000814:39:18.768Bulk or Interrupt Transfer9 bytes buffer
in01:00:81892EB878h
usbsnoop89381BB0h
URB000914:39:18.768Bulk or Interrupt Transfer9 bytes buffer
in01:00:81892436C0hUSBPDO-8
89381BB0h
URB0010-000514:39:18.846Bulk or Interrupt TransferInput Report len:800 00 00 00 00 00 00 00in01:00:81892436C0hUSBPDO-8
89480B80hSuccess (Success)
URB0011-000414:39:18.846Bulk or Interrupt TransferInput Report len:800 00 00 00 00 00 00 00in01:00:81892EB878h
usbsnoop89480B80hSuccess (Success)
URB001214:39:18.846Bulk or Interrupt Transfer9 bytes buffer
in01:00:81892EB878h
usbsnoop89480B80h
URB001314:39:18.846Bulk or Interrupt Transfer9 bytes buffer
in01:00:81892436C0hUSBPDO-8
89480B80h
URB0014-000914:39:27.205Bulk or Interrupt TransferInput Report len:800 00 58 00 00 00 00 00in01:00:81892436C0hUSBPDO-8
89381BB0hSuccess (Success)
URB0015-000814:39:27.205Bulk or Interrupt TransferInput Report len:800 00 58 00 00 00 00 00in01:00:81892EB878h
usbsnoop89381BB0hSuccess (Success)
URB001614:39:27.205Bulk or Interrupt Transfer9 bytes buffer
in01:00:81892EB878h
usbsnoop89381BB0h
URB001714:39:27.205Bulk or Interrupt Transfer9 bytes buffer
in01:00:81892436C0hUSBPDO-8
89381BB0h
URB0018-001314:39:27.299Bulk or Interrupt TransferInput Report len:800 00 00 00 00 00 00 00in01:00:81892436C0hUSBPDO-8
89480B80hSuccess (Success)
URB0019-001214:39:27.299Bulk or Interrupt TransferInput Report len:800 00 00 00 00 00 00 00in01:00:81892EB878h
usbsnoop89480B80hSuccess (Success)
URB002014:39:27.299Bulk or Interrupt Transfer9 bytes buffer
in01:00:81892EB878h
usbsnoop89480B80h
URB002114:39:27.299Bulk or Interrupt Transfer9 bytes buffer
in01:00:81892436C0hUSBPDO-8
89480B80h
0 Kudos
Reply
4,156 Views
Tsuneo
Contributor IV

Increase the wMaxPacketSize for the interrupt IN endpoint into 9.

It is assigned HID_INT_IN_EP_SIZE macro

 

 

Hid.h#define HID_INT_IN_EP_SIZE      9

Where did you change?

On the trace, the device still returns the input report without any report ID.

Revise your code so that you see this report format on the trace.

 

 

For keyboard,offset (byte) 0       report ID (01) 1       modifier keys 2       padding 3 - 8   keycode arrayFor mouse,offset (byte) 0       report ID (02) 1       buttons 2       X asis 3       Y axis

 

 

You run USBlyzer and SnifUsb (usbsnoop) at the same time.

It causes the trace complicated.

 

Tsuneo

 

0 Kudos
Reply
4,155 Views
Tsuneo
Contributor IV

This is another problem from above one.

You are enabling boot keyboard on the interface descriptor.

But it is not supported on your code at all.

 

    /* Interface Descriptor */    {    sizeof(USB_INTF_DSC),   /* Size of this descriptor in bytes   */    DSC_INTF,               /* INTERFACE descriptor type          */    0,                      /* Interface Number                   */    0,                      /* Alternate Setting Number           */    2,                      /* Number of endpoints in this intf   */    HID_INTF,               /* Class code                         */    BOOT_INTF_SUBCLASS,     /* Subclass code                      */  <--------// keyboard:    HID_PROTOCOL_KEYBOAD,   /* Protocol code                      */  <--------// mouse://    HID_PROTOCOL_MOUSE,     /* Protocol code                      */    0                       /* Interface string index             */    },

 1) hid.c handles Get_Protocol and Set_Protocol requests properly, but Current_Active_Protocol is not initialized to report protocol (1) anywhere. Add the initialization to Init_EP_For_HID(), which is called from Set_Configuration handler.

#define HID_PROTOCOL_BOOT     0#define HID_PROTOCOL_REPORT   1void Init_EP_For_HID(void){       ...    ...                                                    // <-------- add this line    Current_Active_Protocol = HID_PROTOCOL_REPORT;  // set to default report protocol    return;}

 

2) While Current_Active_Protocol is boot protocol (0), return this "standard" keyboard report. No mouse report is sent to host.
offset (byte) 0       modifier keys 1       padding 2 - 7   keycode array

 When Current_Active_Protocol is report protocol (1), both of keyboard and mouse reports are sent back in turn, as described above.

 

Tsuneo

 

0 Kudos
Reply
4,155 Views
irob
Contributor V
Tsuneo, many thanks for your gracious help! I now have this project working, both as mouse and keyboard. I've attached the working and cleaned up code here for all to use. As it turns out Current_Active_Protocol is already initialized in function HIDClass_Request_Handler, located in hid.c But your help with the report format was the key to most of my problems. Thanks to USBlyzer, I could see that my reports for mouse and keyboard were both off by one byte, due to the insertion of the ReportID byte at the beginning Very trivial to fix. To all the Freescale devs out there, I've made the Reset switch on the DEMOJM platform board function as my "device switcher", since there are precious few switches to experiment with. While the Reset switch is undepressed, the JS16 functions as keyboard. While depressed, it functions as mouse. If anyone has questions about what I've done, let me know!
0 Kudos
Reply
4,155 Views
AkaLaka
Contributor II

I appreciate the work you did for this, and decided to give it a try.

 

I tried building the zipped code that you posted. I had to fix two errors before it built. HID_RPT_SIZE in hid.h was 63, and needed to be 119 to accomodate the additional mouse stuff. Also in hid.c the definition of HID_Transfer_Rpt was the old definition with two parameters. After fixing these and building it, It doesn't allow me to send keystrokes. I haven't gotten into debugging it yet. But I'm suspicious, since the code that you posted doesn't build, might it be missing some other changes?

 

Thanks again for your efforts.

0 Kudos
Reply
4,155 Views
irob
Contributor V

Akalaka, did you download the zip in my latest message?  Check it out, because I thought I had fixed all the errors you're describing.

 

Unfortunately, after a certain amount of time, use posters are no longer able to edit our messages or delete old attachments.

 

Let me know if the zip file from my ver last post works for you.

0 Kudos
Reply
4,155 Views
AkaLaka
Contributor II

Sorry, my mistake. I think I had the original hid.h file open when I unzipped. It still doesn't work with the keyboard, but I'll take it from here. My apologies.

0 Kudos
Reply
4,155 Views
irob
Contributor V

Huh, weird.  Not sure what state that last zip was in.

 

I just recompiled my latest and tested on the JM16 board.  Both keyboard/mouse work in this version.  See attachment below.

0 Kudos
Reply
4,155 Views
AkaLaka
Contributor II

The sources you previously posted are identical. My problem was with some code that didn't take into account the additional offset on Rpt_Buf. My target is not the eval board, so I had to adapt it to make it work. It's now working fine. Again, many thanks for your efforts!

0 Kudos
Reply
4,155 Views
irob
Contributor V

Ah, very good.  Glad to be of help!

0 Kudos
Reply
4,155 Views
irob
Contributor V

Tsuneo, yes, it's me!  Very clever of you to track me down.  What I found was that I didn't need to delete the device from the Device Manager.  MS Windows found both mouse and keyboard when I inserted onto its USB bus.

 

However, it's the data buffers that aren't working right now.  Thanks for your help regarding the report IDs.  I will see about preceding the data buffer output routines with the report ID.

0 Kudos
Reply