DEMO9S08AW60 and MCF51ACxxx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEMO9S08AW60 and MCF51ACxxx

1,903 Views
thm59
Contributor II
Helllo,

The question is in the title.
Is it possible to try the new MCF51ACxxx with a DEMO9S08WA60, assuming that the P&E firmware will be updated and the MCF51ACxxx is the same ?

thierry
Labels (1)
0 Kudos
Reply
1 Reply

755 Views
Ake
Contributor III
Hello,
If you get the DEMOAC, with the 9S08AC60 top board, you can run your 9S08AC code on it.
If it is written in C, there is a good chance that it will work the first time you replace the 9S08AC60 with a MCF51ACxxx.
If you develop your code using a DEMO9S08AW60 board, you would probably have to rewrite and change some modules in order to get it to run on the DEMOAC board.
 
Regards,
Ake
0 Kudos
Reply