Converting SMAC to Floating Point

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Converting SMAC to Floating Point

2,466 Views
mjcoury
Contributor I
I am running SMAC 4.1c with the Freescale 1392 SARD cards. Is there a way to convert one of those demo projects to floating point?

OR

How do I start a floating point project in codewarrior 3.1 then import the SMAC files?


Thanks

Message Edited by mjcoury on 2006-11-1610:22 AM

Labels (1)
0 Kudos
Reply
1 Reply

1,271 Views
stevasway
Contributor III
A way to convert a demo projects to floating point is to import the right lib under Libs Group.
In a demo project is set to ansiis.lib, you should replace it and use ansifs.lib.

The libs in my machine are located at
C:\Program Files\Metrowerks\CW08 V3.1\lib\hc08c\lib

Bye
Stevasway
0 Kudos
Reply