Contiguous Flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Contiguous Flash

1,394件の閲覧回数
rdazcal
Contributor III

Greetings,

 

The MC9S08LC36 MCU has two Flash memories that are not contiguous.

 

Do I have to worry if my program is placed in between the memories as if it were a contiguous memory space?

ラベル(1)
0 件の賞賛
返信
1 返信

1,077件の閲覧回数
bigmac
Specialist III

Hello,

 

The contents of the PRM file for the project enable the linker to determine which address ranges are read-only, for the purpose of placing code.

 

The one exception is an absolute assembly project, where the linker is not used.  Here it is the responsibility of the programmer to determine a suitable code placement.

 

Regards,

Mac

 

0 件の賞賛
返信