Compiler and schematics program for  MC68HC908JB8JPE ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Compiler and schematics program for  MC68HC908JB8JPE ?

5,723件の閲覧回数
quangpk
Contributor I
Hi every body,
- I am beginer studying 8 bit microcontroller of Motorola, I have partnumber MC68HC908JB8JPE. What compiler can use for this ? What schematics program can use ?
Regards,
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,995件の閲覧回数
J2MEJediMaster
Specialist I
You can go to the product page on the Freescsle web site to track down documentation on the part and application notes. Enter the part number, MC68HC908JB8, in the part number box at the upper right of this page and click on the arrow. You should be able to use CodeWarrior to write in C for programming this part.

---Tom
0 件の賞賛
返信

1,995件の閲覧回数
YY
Contributor I
Hi,
I'm new in this too, but I'm actually using the same controller MC68HC908JB8 for my application. It's similar to RD68HC908USBMKEYBD, that i've seen in the freescale website reference design section. I've downloaded all the relevant documentations also the source code provided. I've also installed the Code Warrior V5.0 for this application. However, I have problems compling the example code in the CW. I'm not sure what happen, but i'm trying to look into it. Is there anyone tried this example code provided before?
 
Thanks & Regards,
0 件の賞賛
返信

1,995件の閲覧回数
quangpk
Contributor I
Pls, introduce to me what program (work in Win2k) can work with my circuit to load flash to MC68HC908JB8,
Best Regards,
 
Message Edited by t.dowe on 2009-09-16 10:09 AM
0 件の賞賛
返信