Compiler and schematics program for  MC68HC908JB8JPE ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compiler and schematics program for  MC68HC908JB8JPE ?

5,719 Views
quangpk
Contributor I
Hi every body,
- I am beginer studying 8 bit microcontroller of Motorola, I have partnumber MC68HC908JB8JPE. What compiler can use for this ? What schematics program can use ?
Regards,
Labels (1)
0 Kudos
Reply
3 Replies

1,991 Views
J2MEJediMaster
Specialist I
You can go to the product page on the Freescsle web site to track down documentation on the part and application notes. Enter the part number, MC68HC908JB8, in the part number box at the upper right of this page and click on the arrow. You should be able to use CodeWarrior to write in C for programming this part.

---Tom
0 Kudos
Reply

1,991 Views
YY
Contributor I
Hi,
I'm new in this too, but I'm actually using the same controller MC68HC908JB8 for my application. It's similar to RD68HC908USBMKEYBD, that i've seen in the freescale website reference design section. I've downloaded all the relevant documentations also the source code provided. I've also installed the Code Warrior V5.0 for this application. However, I have problems compling the example code in the CW. I'm not sure what happen, but i'm trying to look into it. Is there anyone tried this example code provided before?
 
Thanks & Regards,
0 Kudos
Reply

1,991 Views
quangpk
Contributor I
Pls, introduce to me what program (work in Win2k) can work with my circuit to load flash to MC68HC908JB8,
Best Regards,
 
Message Edited by t.dowe on 2009-09-16 10:09 AM
0 Kudos
Reply