Coding the MC9S08QG8_16

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Coding the MC9S08QG8_16

2,155 Views
gdesmedt1
Contributor I

Hi guys... I've been handed a project and I need to continue coding the chip... MC9S08QG8_16 and the problem is that processor expert in CodeWarrior tells me that the CPU aint supported.

 

I've visited Processor experts' site and can't seem to download the necesarry CPU bean!

 

I'm using CodeWarrior 5.6 with Processor Expert 2.94.. I know it's old but I need to get this project going A.S.A.P!

 

Can ANYONE please help me.. or e-mail me the neccessary files.. PLEASE!

Labels (1)
0 Kudos
Reply
2 Replies

1,342 Views
bigmac
Specialist III

Hello, and welcome to the forum.

 

Are you attempting to use the 8-bit MCU version or the 16-bit MCU version of CW?  Since you have posted in the 16-bit forum, and the MC9S08QG8 is actually an 8-bit device suggests that you might be using an inappropriate version.

 

You will probably need to download the latest (8-bit) version of CW, or install updates to an older version, so that the device is supported (although the QG8 is not new, and has been around for quite some time).

 

Regards,

Mac

 

0 Kudos
Reply

1,342 Views
gdesmedt1
Contributor I

Hi Bigmac,

 

Thanks for the welcome, and yes.. it seems I have stumbled into the wrong forum!

 

I have reposted this into the hopefully now correct forum here.

 

Have included an update in the post.. maybe info might help ppl understand what i need!

 

Thanks mate!

0 Kudos
Reply