Codewarrior Professional Edition = more efficient code?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior Professional Edition = more efficient code?

1,783 Views
blitzamit
Contributor I

Hello,

 

Is it so that the compiler that comes with Codewarrior Professional Edition is different from the one that comes with Special Edition? In other words, is it so that by using Codewarrior Professional Edition results in a more efficient use of microcontrollers memory (RAM, ROM) by using better optimization routines as compared to using Special Edition?

 

I know that Special Edition has restrictions pertaining to code size, want to know if there are restrictions pertaining to code optimization.

 

Thanks,

Amit

Labels (1)
0 Kudos
Reply
2 Replies

1,631 Views
NavidadRedivivu
Contributor III

Short answer to this one: it's the same compiler (afaik). The only restrictions between the different editions pertain to code size.

0 Kudos
Reply

1,631 Views
J2MEJediMaster
Specialist I

The compiler and linker in the Special Edition are identical to those in the other CodeWarrior editions.

 

---Tom

0 Kudos
Reply