Codewarrior 10.6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Codewarrior 10.6

8,485 次查看
detlefwohmann
Contributor II
Hello
I am writing a program in CW10.x
and I use an RTC and MTIM.
      ISR(RTC_INT)
      {
    RTCSC_RTIF = 1;
      }

     ISR(TIMER_OF)
      {
    MTIMSC_TOF = 0;
      }

compile the program and save all.

Everything is OK.
Then I do exit
and start the program again and everything is gone
Description Resource Path Location Type
Symbol TIMER_OF in file E:/Workspace 9S08/Sonora_v2/FLASH/Generated_Code\Vectors_c.obj is undefined Sonora_v2 C/C++ Problem
Symbol RTC_INT in file E:/Workspace 9S08/Sonora_v2/FLASH/Generated_Code\Vectors_c.obj is undefined Sonora_v2 C/C++ Problem
mingw32-make: *** [Sonora_v2.abs] Error 1 Sonora_v2 C/C++ issue

is there a solution

Thanks.
10 回复数

8,461 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Sorry what is the part number that you are using?

8,409 次查看
detlefwohmann
Contributor II

I am using 9s08sh

Best regards

D.Wohmann

8,398 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Please close the project that you are using and create a new workspace.

 

After you create a new workspace, please create a new project and check that on this new project all is correct.

8,378 次查看
detlefwohmann
Contributor II

Hello Vicente Gomes
Unfortunately I have the same problem.
If I use a KL25Z I have no problems.
I've been writing programs in asm for 30 years.

I also tried version 11.1 on another LAPOP 32bit but it's the same.
I think I should keep writing in asm programe.
Thanks Regards
D.Wohmann

8,372 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

sorry I did not get what you need, Do you want to create an asm code for the s08sh 

 

if this is the case I just create an empty code

 

8,345 次查看
detlefwohmann
Contributor II

Hello Vicente
my case is not the program in asm, but I wanted to write a program in c and use the Procesor expert.
I installed cw 11.1 in 4 different ones and they all have the same error.

I wonder if I'm at fault.

If you want I'll tell you exactly what I'm doing.

google translate
Best regards
D.Wohmann

8,444 次查看
detlefwohmann
Contributor II

Hello
Thank you for your reply.
I don't understand what part number you need.
I have installed
Code Warrior Development Studio for Microcontrollers

Version: 10.7
Build: 160721

Best regards
D.Wohmann

8,432 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Are you using S08 family, Kinetis, S12 etc?

 

6,686 次查看
Frank_Wang2024
Contributor II

Hello,

I am using Codewarrior 10.6, but I can't find the download link, it was replaced by version 11.1. Because of some legacy configuration, I need to use the 10.6 version. Could you provide the download link for 10.6 version?

B/Rs

 

 

 

8,408 次查看
detlefwohmann
Contributor II

Yes i am using 9s08 and Kinetis KL25z

Best regards

D.Wohmann