CodeWarror

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarror

Jump to solution
1,210 Views
Julian99
Contributor III

Does anyone know where I can download a copy of CodeWarrior for 8-bit processors that will run under Linux (Ubuntu)? A general enquiry showed that C/W does run under linux, but all of the links are for windows.

Tags (2)
0 Kudos
Reply
1 Solution
1,167 Views
luis_maravilla
NXP Employee
NXP Employee

Hello,

Sorry for the inconveniences, the available version of CodeWarrior for 8-bit processors [CodeWarrior v11.1] is not available for Linux only windows.

Best Regards, Luis

View solution in original post

0 Kudos
Reply
2 Replies
1,167 Views
luis_maravilla
NXP Employee
NXP Employee

Hello,

Sorry for the inconveniences, the available version of CodeWarrior for 8-bit processors [CodeWarrior v11.1] is not available for Linux only windows.

Best Regards, Luis

0 Kudos
Reply
393 Views
Julian99
Contributor III

I know that! I have been using CW for "many years", running under Windows 7 which is running under Dropbox which is running under OSX on my Intel-based MAC. All I want is to do the same thing on my new ARM-based MAC. So far I have installed Dropbox and loaded Windows 11. (earlier versions of Windows are not compatible with the new MACs). I have installed CW 11.1 in Windows and it works.

As I said in my original post CW does not recognise the Multilik debug probe because there is no device driver installed. Please refer to my original post for details of what is required 

0 Kudos
Reply