Code WArrior support for the s08DV Family

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code WArrior support for the s08DV Family

1,691 Views
Mobileye
Contributor I

Does any one know how to use the CodeWarrior for the MC9S08DV family?

(I don't find it there)

Message Edited by Mobileye on 2006-11-0906:32 AM

Labels (1)
0 Kudos
Reply
1 Reply

1,016 Views
mayfly
Contributor III
I have just started to use the s08D(Z) Family as an alternative to the HC08GZ for CAN. The DZ (not the HC08GZ) is essentially the same as the DV. You have to add updates for Codewarrior (look for something like S08Dx on the update site...or check for updates with Codewarrior) which will get you standard compiler support and header/library files for the microcontrollers. Processor Expert/Device Initialization doesn't seem to be supported yet (as of 2007-1-20). I am not sure what else is missing. I am using the Demo DZ60 board (DEMO9S08DZ60) and have a C version of the blinking led working using Codewarrior (with the updates). The Demo board only comes with an asm example, so there's no learning by example to be had.

Message Edited by mayfly on 2007-01-2005:59 AM

Message Edited by mayfly on 2007-01-2006:00 AM

0 Kudos
Reply