Code WArrior support for the s08DV Family

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code WArrior support for the s08DV Family

1,684件の閲覧回数
Mobileye
Contributor I

Does any one know how to use the CodeWarrior for the MC9S08DV family?

(I don't find it there)

Message Edited by Mobileye on 2006-11-0906:32 AM

ラベル(1)
0 件の賞賛
返信
1 返信

1,009件の閲覧回数
mayfly
Contributor III
I have just started to use the s08D(Z) Family as an alternative to the HC08GZ for CAN. The DZ (not the HC08GZ) is essentially the same as the DV. You have to add updates for Codewarrior (look for something like S08Dx on the update site...or check for updates with Codewarrior) which will get you standard compiler support and header/library files for the microcontrollers. Processor Expert/Device Initialization doesn't seem to be supported yet (as of 2007-1-20). I am not sure what else is missing. I am using the Demo DZ60 board (DEMO9S08DZ60) and have a C version of the blinking led working using Codewarrior (with the updates). The Demo board only comes with an asm example, so there's no learning by example to be had.

Message Edited by mayfly on 2007-01-2005:59 AM

Message Edited by mayfly on 2007-01-2006:00 AM

0 件の賞賛
返信