Clock setting and IEEE 802.15.4 on MC13213

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clock setting and IEEE 802.15.4 on MC13213

1,250 Views
venca
Contributor I
Hi,

I want to run IEEE 802.15.4 stack. Is it necessary to have the MCU clock driven from external CLK0? Or can I use the internal MCU clock at ~17.5 MHz?

Thanks for your response.
Labels (1)
0 Kudos
Reply
1 Reply

721 Views
Mads
Contributor V
venca,
 
It is possible to run on a different clock source, but that means you will have to provide 2 crystals to the IC, one for the radio and one for the CPU. also you would have to modify the timer modules, and clock initilization and other modules that are dependent of the clock your self to make sure the system is running.
 
the best is to stay with the reference design and use the clk0.
 
Br,
Mads
0 Kudos
Reply