Clock generation without external parts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clock generation without external parts

3,179 Views
WimmerChris
Contributor I
Hello everybody,
 
i've a short question: Which HC08 MCUs like the QT4 or QB8 have an internal oszilatior, so that i can run them with out external parts?
 
 
Thanks for help!
With best regards
 
Christian Wimmer
Labels (1)
0 Kudos
Reply
4 Replies

2,177 Views
peg
Senior Contributor IV
Hi Chris,
 
This document helps:
 
 
The clock type column gives the acronym for the clock module type, from there and from a few checks you should be able to work it out. They don't make it real easy, do they?
 
0 Kudos
Reply

2,177 Views
WimmerChris
Contributor I
Hi Peg,
 
thanks for the overview it's pretty good. But i'm sorry it doesn't help me in my problem because, if you look at the QT4A or the QB4 for example you will see that there is a "OSC" at the clock type. (Both devices have an internal oscillator.) But the JL8 (there is also a "OSC" ) didn't have an internal oscillator.
 
Thanks for your help.
Best regards.
Christian


Message Edited by WimmerChris on 2007-05-09 06:48 PM
0 Kudos
Reply

2,177 Views
peg
Senior Contributor IV
Hi Chris,
 
I know my response was fairly useless. I made in in the vain hope that someone at Freescale would see it and realise that filling these tables with useless, company specific acronyms only serves to keep the $%^&*'s in the marketing department happy and does nothing to assist its users.
 
0 Kudos
Reply

2,177 Views
bigmac
Specialist III
Hello Chris,
 
The HC908 devices that have a trimmable internal oscillator are limited to a few series only - Qx series, EY, GT, but not many others come to mind.  A few other series do have an internal oscillator, but is not accurate or stable with voltage and temperature.
 
Trimmable internal oscillators seem much more prevalent within the various 9S08 series, which are more recent devices.
 
Regards,
Mac
 
0 Kudos
Reply