Clock Sources on MC1321x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Clock Sources on MC1321x

2,790件の閲覧回数
stevasway
Contributor III
Is it possible to connect both clock source on MC1321x
in order to use 16MHz when radio modem is on, and 32kHz when
I switch off the radio and run only the S08 micro section?

To obtain ultra low power, I need to switch on the radio modem
only when I need, but I need a S08 section running without
using internal (not exact) clock sources.

Stevasway
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,765件の閲覧回数
stevasway
Contributor III
Strikecity,

if you see at paragraph 3.5 look at Figure 3-3. MC1321x Clock Connections,
I don't understand if it's possible to connect both clock sources.
Probably if both clock sources are connected you can't make the connection
between pin 9 and 10, but the S08 section has 32kHz source and radio has his 16MHz
clock source.

Doubts about the synchronization between radio and S08.....

Stevasway
0 件の賞賛
返信

1,765件の閲覧回数
strikecity
Contributor I
stevesaway,

I'm looking at pages 7 and 9 of the MC1321x datasheet... it looks like the 16MHz radio crystal only drives the S08 core if pins 9 and 10 are connected. If you don't make this connection, you can drive the core at any frequency.
0 件の賞賛
返信