Choosing real time clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Choosing real time clock

5,631 Views
santosh
Contributor I
We are using MC9s08GT and want to use an rtc.
But witch one is the best clock? Make it sense to use the I2C Interface? The SPI is allready used.

Thanks for help.
Labels (1)
0 Kudos
Reply
3 Replies

1,766 Views
Wings
Contributor I
If really low power is a requirement, check out the DS2417. 1-wire interface & programmable pulse output. Draws around 180 nanoamps @ 3v. Doesn't have clock registers, just a 32-bit count of seconds so you'll have to do your date & time thing in software.
0 Kudos
Reply

1,766 Views
Encoder
Contributor I
I have been using a PCF8583 on my old HC705B controller for years, with a synthetic IIC from 2 I/O lines, and one of the 2 was multiplexed with another peripheral.
 
Perhaps today I would use the DS1337 which seems to be newer and cheaper. It too uses IIC.
 
Encoder
0 Kudos
Reply

1,766 Views
mke_et
Contributor IV

I'm using the DS1307Z on my new design.  It's I2C and seems pretty simple to implement.

Mike

 

0 Kudos
Reply