Changing the processor from MC9S08GT60 to MC9S08ac128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Changing the processor from MC9S08GT60 to MC9S08ac128

837件の閲覧回数
preetuabraham
Contributor III

Hi,

I am working on a project which had used MC9S08GT60 processor and the complete loadable file was less than 64kb.Now I changed to MC9S08ac128 processor so that we have more memory space. I am not sure whether I have to use Banked memory model or small memory model since I moved to MC9S08AC128.The code remains same. If I use banked memory model ,whether I have to do any changes specifically for banked memory model .whether the PRM file only needs to be modified .

0 件の賞賛
返信
0 返答(返信)