Can't Program or Enter Debug Mode on a MC9S08QE32

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't Program or Enter Debug Mode on a MC9S08QE32

ソリューションへジャンプ
2,441件の閲覧回数
Designer11
Contributor IV

Hi Guys,

 

I'm desperately needing your help on this issue. I designed a board with a QE32 uController and every time I used either the USB multilink or Multilink Universal I can't program the board or get the board to enter debug mode. The two Multilinks work great with the QG8 series.

 

On the other hand, when I use the cyclone Pro with the board it enters debug mode and able to program the board without any problem. What I did for a test was I toggle a port on the MCU.

 

BR,

D 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,993件の閲覧回数
Designer11
Contributor IV

I don't know why the QE32 microcontroller required the VDD Line to connect to the programming header, even if you are not using the Vdd voltage on the programmer header to power the target board.  But You have to connect it from the target board to your Multilink programmer,

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,994件の閲覧回数
Designer11
Contributor IV

I don't know why the QE32 microcontroller required the VDD Line to connect to the programming header, even if you are not using the Vdd voltage on the programmer header to power the target board.  But You have to connect it from the target board to your Multilink programmer,

0 件の賞賛
返信
1,993件の閲覧回数
kef
Specialist I

Multilink is multivoltage tool. Since Vdd range is as big as 5 to 2.7V or even less, you need to provide your target Vdd to Multilink to make it able to convert logic levels to internal Multilink levels properly.

0 件の賞賛
返信
1,993件の閲覧回数
Designer11
Contributor IV

Kef,

 

Thanks for the explanation.

 

BR,

D

0 件の賞賛
返信