Can JTAG on NXP ARM MCUs be used for programming?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can JTAG on NXP ARM MCUs be used for programming?

3,011 Views
phirung
Contributor II

I'm evaluating the LPC11U6x family for a low-volume hobbyist project, but will automate PCBA production. A common approach is to use JTAG to verify the PCBA and upload code. JTAG is briefly described in the family datasheet.

However, there's no mention of the ability to use JTAG to upload code. If this is not possible, can code be uploaded as a final production step via an external hardware interface rather than using the internal bootloader?

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

2,975 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Phirun Ng,

You may use JTAG to upload the code to your device. You may find more details on how to connect using JTAG on the following Community Document.

https://community.nxp.com/thread/388998 

I hope that this helps!
Regards,

Gustavo

0 Kudos
Reply

2,975 Views
phirung
Contributor II

Thanks for the advice and the link. Am still working through initial docn and finding my way around the site. All looking very promising.

0 Kudos
Reply