Can JM60's S08ACMPV2 be used as a linear amplifier?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can JM60's S08ACMPV2 be used as a linear amplifier?

ソリューションへジャンプ
2,245件の閲覧回数
z_george
Contributor I
ラベル(1)
0 件の賞賛
返信
1 解決策
1,577件の閲覧回数
ok2ucx
Contributor IV

No, at least not as a standard opamp. The external signal ACMPO is a digital output, so it tends to slip either to Vdd or Vss depending on the actual analog level of ACMPO (internally). Thus you can't close the feedback via standard resistor network.

 

I've tested that, also wanted to use that opamp similarly. 

 

Pavel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,578件の閲覧回数
ok2ucx
Contributor IV

No, at least not as a standard opamp. The external signal ACMPO is a digital output, so it tends to slip either to Vdd or Vss depending on the actual analog level of ACMPO (internally). Thus you can't close the feedback via standard resistor network.

 

I've tested that, also wanted to use that opamp similarly. 

 

Pavel

0 件の賞賛
返信
1,577件の閲覧回数
z_george
Contributor I
Hi Pavel, thanks a lot for your information. I guess I mixed the MJ60 ACMPOV2 with Operational Amplifiers on MSP430Fxx. – The on chip Amplifier is useful especially for sensor applications.
0 件の賞賛
返信