Can I use the printf() for print my debug information? - MC13211

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use the printf() for print my debug information? - MC13211

2,777 Views
Beijing2008
Contributor I
Dear all:
 
   I would like to insert several printf() statement in C source code of Codewarrior project,that for output debug information in debug windows,like the VC++ compiler,is it possible?how to do?
 
  second problems:
  Where I can find the read/write flash memory examples?My applicaiton based on the SMAC codebase with MC13211,because I want to save a constant to flash memory!
 
Best regards,
Charly
 
 
 
Added p/n to subject.


Message Edited by NLFSJ on 2008-06-30 02:28 PM
Labels (1)
0 Kudos
Reply
3 Replies

1,781 Views
Beijing2008
Contributor I
Hi all:
 
   what's mean of "Added p/n to subject. " at the post tail?
 
Best regards,
 
Charly
 
0 Kudos
Reply

1,781 Views
peg
Senior Contributor IV
Hi Charly,


Beijing2008 wrote:
Hi all:
 
   what's mean of "Added p/n to subject. " at the post tail?
 
Best regards,
 
Charly
 



This simply means that one of our friendly moderators has added the part number of the device you are talking about onto the end of your subject line (- MC13211). This makes your post and other followups more accessable for others in the future.
It also gives you a hint to put it there yourself next time.


0 Kudos
Reply

1,781 Views
Beijing2008
Contributor I
Hi all:
 
Via study ,Now I use the debugger tools of CodeWarrior for debug C code,mainly use the Memory or Command windows!
 
However,I still don't clear that how to read/write the flash memory of MC13211,Can you  provide a simple demo example to me?
I tried to read the MC1321x datasheet about flash memory,but it is difficult to me and my project schedule is urgent, please give me some helpness!
 
Thanks and best regards!
 
Charly
 
0 Kudos
Reply