Calling Firmware Functions in FXTH87xxDD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Calling Firmware Functions in FXTH87xxDD

1,460件の閲覧回数
f20150335
Contributor III

Hi, i cannot get the result in the register when I am multiplying two numbers using the following code - 

pastedImage_1.png

Am I completely incorrect in calling the function. How should it be done?  When i write TPMS_MULT_SIGN_INT16 I get an error message too. So what should I do to call this function?

I am only implementing this function for learning as later I would have to call the read_pressure type functions too.

0 件の賞賛
返信
0 返答(返信)