CAN & USB?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN & USB?

3,659 Views
jafriede
Contributor II

We are using the 9s08DZ60 in a recreational vehicle application utilizing the CAN bus.  We would like to add USB capability to retrieve diagnostics to a notebook PC but I do not see a flavor of the 9s08 that has both USB and CAN.  One possible solution I see is a company called FTDI that makes a USB - RS232 solution.  Does anyone have any other suggestions?

 

http://www.ftdichip.com/

Labels (1)
0 Kudos
Reply
4 Replies

2,516 Views
jag
Contributor IV

CP2102

 

Bye Jack 

0 Kudos
Reply

2,516 Views
bigmac
Specialist III

Hello,

 

You could make use a "standard" off-the-shelf RS232 to USB adaptor lead. This lead might incorporate the FTDI device, or another similar USB device.

 

Regards,

Mac

 

0 Kudos
Reply

2,516 Views
jafriede
Contributor II

bigmac wrote:

Hello,

 

You could make use a "standard" off-the-shelf RS232 to USB adaptor lead. This lead might incorporate the FTDI device, or another similar USB device.

 

Regards,

Mac

 


That would certainly work, but I don't want my customers to have to buy extra hardware.

 

Thanks

0 Kudos
Reply

2,516 Views
kef
Specialist I
Does it have to be automotive chip? Have a look at MCF51JM. Unfortunately MSCAN is present only in Coldfire JM, not in S08 JM.
0 Kudos
Reply