Bootloader.exe (v5.32) - Error starting API! message from cmd line

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bootloader.exe (v5.32) - Error starting API! message from cmd line

2,795件の閲覧回数
dukdevguy
Contributor I
I'm trying to flash one of our MC1312x devices - and to ease some of our support dept issues to update a few of our devices using the command line version of TestTool - Bootloader.exe.  While the GUI TestTool works fine in flashing the new .s19 files - using Bootloader.exe with the same devices & s19 returns the message "Error starting API!"
 
The simple test with bootloader.exe has been:
c:\program files\freescale\test tool\s19> bootloader.exe testConfigWBLv1.4.s19 /C COM3
The rest of the defaults (baud @ 19200, evk_embedded_bootloader.bdm s.b. fine)
 
Something simple I'm overlooking?  Another (better) way to offer a cmd line flash of the s19?
 
Thanks!
ラベル(1)
0 件の賞賛
返信
1 返信

1,460件の閲覧回数
RickN
Contributor I
Hi,
 
   I used the boot loader described in AN2295 for another 9S08 MCU and it worked on the first shot.  Decent Windows app included that might be appropriate for your situation.
 
 
   The 1312x would have the 9S08GT MCU. 
 
   Thanks,
 
      Rick
0 件の賞賛
返信