Bootloader AW32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader AW32

4,432 Views
Sany
Contributor III
Hi everyone,
 
 I am looking for the bootloader for AW32. AW32 is new to me though I learned basic of GP32 before. I had the bootloader for GP32. If the source isn't available, I am thinking of writing one my own. Is the GP32 bootloader suitable to be modified for AW32 bootloader? Or is there better option?
Labels (1)
0 Kudos
Reply
3 Replies

2,033 Views
ok2ucx
Contributor IV
Hi there,
 
I would suggest to look at AN2295SW rev.8 that has been released on the freescale web recently. S08AW family is now supported.
 
Regards, Pavel
 
Freescale Roznov p.R., Czech Republic
0 Kudos
Reply

2,033 Views
Sany
Contributor III
ty for the reply, got the file now :smileyvery-happy:
0 Kudos
Reply

2,033 Views
PANOSSO
Contributor I

He there Sany . . . . .

. . .i do whanted to use also a bootloader on my application with AW32, and I´m also using the AN2295SW to do it . . .but . . .I facing a problem that I am able to do one time only the boot loader process . .  .

 

I know that I was supose to protet the boot loader region in my app, but as I undestand I´m doing this by the modifications I made on my Project.prm (please take a look at attachment)

 

Can you give me a help how to sove my problem ??

 

best brazilian regards

 

 

 

0 Kudos
Reply