BootLoader - timeout

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

BootLoader - timeout

4,086 次查看
Iggy
Contributor I
Hello,
I use Embedded Bootloader 5.00 (part of Test Tool v.9.1), but I can´t load the application into mc9s08gt60 (as part of ZigBee pack - mc13193 evaluation kit). Bootloader gives me these messages: "Timeout waiting for download firmware to complete!" or "Timeout waiting for s19 start transfer to complete!". There´s no option to change timeout value. I try programming through UART, USB and BDM (I know the whole flash is erased while BDM programming, so MAC and bootloader too)- the same (bad) result. What can be wrong? It´s problem with hardware?
I try load program into micro with P&E USB Multilink. This loader said me: "that loading was complete", but there´s no activity of micro.
Can somebody help me, please.

Thanx, Iggy
btw: sorry for my "English"
标签 (1)
0 项奖励
回复
2 回复数

1,923 次查看
Iggy
Contributor I
Another idea:
SMAC User´s Guide, Rev. 1.2, Chapter 3, page 3-3, there´s diagram of possible solution.
Good luck for everybody,
Iggy
0 项奖励
回复

1,923 次查看
Iggy
Contributor I
So, simple solution (of simple problem :-)) - install Test Tool version 9.2. There´s a option programming throught BDM interface..
Regards, Iggy
0 项奖励
回复