Blinking across multiple PCA9745B LED drivers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Blinking across multiple PCA9745B LED drivers

ソリューションへジャンプ
1,789件の閲覧回数
oliverebert
Contributor I

Hello,

we're using two (SPI-)daisy-chained NXP PCA9745B LED drivers and want to blink some LEDs synchronously on both ICs.  The respective LEDs of each driver are associated with a LED group that is configured identically on both ICs.  The gradation start command is issued simultaneously to both ICs.  While the LEDs on each IC are blinking in sync (as expected), the blinking frequencies between different ICs seem to differ and the blinking LEDs diverge pretty quickly!  I don't see any facilities for synchronizing multiple drivers (except for using the /OE pin for external dimming/blinking?)... am I missing something?  Is this use case even supported by the drivers?

How would one go about blinking LEDs synchronously across multiple PCA9745B LED drivers?

Thanks and regards

Oliver

0 件の賞賛
返信
1 解決策
1,596件の閲覧回数
oliverebert
Contributor I

An FAE from our distributor confirmed that it is indeed not possible to synchronize two or more PCA9745Bs to achieve e.g. synchronous gradation operation as described above.  This is due to the spread of the 8 MHz internal oscillator frequencies across different ICs (presumably 20--30%?), and an input for an external clock is not available.  Anyway, this seems like a missed opportunity ...

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,597件の閲覧回数
oliverebert
Contributor I

An FAE from our distributor confirmed that it is indeed not possible to synchronize two or more PCA9745Bs to achieve e.g. synchronous gradation operation as described above.  This is due to the spread of the 8 MHz internal oscillator frequencies across different ICs (presumably 20--30%?), and an input for an external clock is not available.  Anyway, this seems like a missed opportunity ...

0 件の賞賛
返信