Bit manipulation of High page registers in 9S08

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bit manipulation of High page registers in 9S08

1,576 Views
Sangram
Contributor I
Hello everybody,
                      I read thred started by andie and answered by David. But, that was not sufficient to clear my doubt about instruction or way in C language , which we use for bit manipulation.
 
                    Shall we use
                                          Registername_bitname = 1 or 0.
        or
                                         Registername = (use & or | for resetting or setting bit)
 
Finally for compiler and execution of program which one of them is more efficient ?
 
 
Labels (1)
0 Kudos
Reply
1 Reply

591 Views
CompilerGuru
NXP Employee
NXP Employee
As far as code efficiency goes, if you expect the operation to be performed to be the same, then I would expect the compiler to generate the same code, hence no difference in runtime efficiency.
If that's not the case, then the compiler should be improved for the less efficient pattern, and not the user code.

Anyway, I think the decision what to use should be based on other criteria than the generated code.
Basically using bitfields has generates more readable C code.
There are also a couple of possible bugs when using masks which dont happen with the bitfield approach.
For example the code could use the bitmask for one register with the address of another one, or the & used in masking is common source of precedence bugs (I mean the "Reg & MAK == 0" type of bugs).
So the mask approach is often done with a bunch of macros, but that has its own drawbacks too.
The drawback of bitfields is that they are by the C language definition compiler dependent. If you use a header file delivered with the compiler, then that is not an issue, but if you want to program independent of the used compiler, then using bitfields is at least conceptually not an option.

BTW, using the mark you should use

Registername |= MASK_OF_BIT;
Registername &= ~MASK_OF_BIT;

Daniel
0 Kudos
Reply